Technical FAQs

Ask a Question

Does PowerLogic PM5000 series meter has Instrument Transformer correction (ITC) feature. If not, which meter model has ITC this feature.

Instrument Transformer Correction (ITC) allows you to correct for inaccuracies in the current transformers (CTs) and potential transformers (PTs).
 
The ITC feature is not available with PowerLogic PM5000 series meter's.
 
ION7550/ION7650 meters are shipped with ITC-capable firmware, its ITC modules (Instr Xformer in the firmware) must be configured using accurate
measurements to ensure valid calculations. There is one Instr Xformer Correction module for each current and voltage input into the meter.
Was this helpful?
What can we do to improve the information ?