Technical FAQs

Ask a Question

What is the different between running the self test "automatically" and "manually by pushing T button" on IM400 vigilohm device.

 The both test are the same i.e. by running the self "automatically" and " Manually at any time by pressing the T contextual menu button on one of the system insulation monitoring screens" of IM400 vigilohm device.
 
Was this helpful?
What can we do to improve the information ?