Technical FAQs

Ask a Question

What are Auxillary Power supply options for Com'X200 Energy Server.

 The Com'X200 comes with 3 ways to get powered:
  1. 100 -> 230VAC (+/- 15%)
  2. 24VDC (+/- 10%)
  3. PoE


Was this helpful?
What can we do to improve the information ?