Technical FAQs

Ask a Question

What is the heat dissipation value from Twido PLC during working condition.

The heat dissipation is equal to the maximum power, for the Twido PLC CPU model TWDLCDA24DRF it is 8.7 W, similarly for the other CPU models like TWDLCDA10DRF it is 3.9 W. 
Was this helpful?
What can we do to improve the information ?