Technical FAQs

Ask a Question

We are getting this error " The Hardware platform does not match the target type or access is denied. Download has been stopped" every time when try to download the program to HMIS5T.

This error mostly occured if you were using wrong part number in the Target Properties like mostly customers use HMISTU855 instead of HMIS5T , we recommend to kindly re-check the target part numbers from the physical device. 
Was this helpful?
What can we do to improve the information ?