Technical FAQs

Ask a Question

Can I connect Vijeo Historian with an existing Vijeo Citect Lite SCADA as a data source.

Vijeo Citect SCADA must have CtApi connection available to connect to Historian. In case if you have already VJC lite license key then you need to confirm this from the existing license key deatils if it has Ctapi license. Otherwise you must choose a SCADA license, that support CtApi or else he can purchase a CTAPI connector license VJC 104288 which can be added to his existing VJC lite license key. 
Was this helpful?
What can we do to improve the information ?