Technical FAQs

Ask a Question

Which software I need to use for program development in SCU8B5.

This SCU8B5 is a combination of both HMI & a PLC controller so using Somachine Software you can create logic programming and download both PLC program as well as HMI screens . Vijeo Designer is also used only for screen development which is already installed when you install SoMachine Software on your system.You can use Somachine version 3.1 with Vijeo Designer version 6.1 Service Pack-3 onwards to work on HMI SCU8B5
Was this helpful?
What can we do to improve the information ?