Technical FAQs

Ask a Question

What is the use of USB port in SCU8B5, is it only used for firmware download.

Yes USB port in SCU8B5 is only used as application port using which you can download firmware or application program in SCU machine controller. 
Was this helpful?
What can we do to improve the information ?