Technical FAQs

Ask a Question

With Vijeo Citect version 7.20 , in runtime I`m not be able to acknowledge alarm. What is the reason for this problem.

From VJC 7.20 onwards you need to confirm that you have created a User linked with a Role with atleast privilege of 1 and then logged in with that user during runtime and then only you can be able to acknowledge the alarms . This behaviour is due to the security enhancedments from VJC version 7.20 onwards.
Was this helpful?
What can we do to improve the information ?