Technical FAQs

Ask a Question

What is the Altivar drives state when the auto decel ramp adapt feature bRA is engaged?

Issue:
What is the drives state when the auto decel ramp adapt feature bRA is engaged?
Product Line:
Alitvar ATV61, ATV71, ATV312, ATV31, ATV58, ATV12
Environment:
All
Cause:
Needs to know the status of the drive when auto decel ramp adapt is activated.
Resolution:
When the stop order is given, the drive state is "DEC" and if this is needed (brA=Yes) the drive will raise the deceleration time but the state stays to "DEC" until the motor is stopped then the state goes in "rdY".

 
Was this helpful?
What can we do to improve the information ?