Technical FAQs

Ask a Question

Is Altivar 71 drive accepts pulse input reference.

Altivar 71 drive with optional Extended I/O card VW3A3202 accepts pulse input reference. This card accepts pulse input reference of 24V/0-30kHz.
Was this helpful?
What can we do to improve the information ?