Technical FAQs

Ask a Question

What is PRA on Altivar 71 drive.

PRA is Power Removal Function Active (drive locked out).
It is a state of the drive which means that it is locked. If  drive displays PRA, that means that you do not have 24 V on the terminal PWR. Normally, all the drive are delivered with a "link" between  terminals PWR and +24.
 
This situation is for safety reason. When the status of ATV71 is PRA, for safety reason, the software is freezed and nothing is done until PWR and +24 are shunted.
 
The solution is to shunt PWR and +24 before power on the drive.
Was this helpful?
What can we do to improve the information ?