Technical FAQs

Ask a Question

What is the minimum voltage required for the functioning of Test button of Acti9 RCDs.

The Acti9 RCD devices are compliant with the standards (IEC/EN 61008 & 61009) that mean -10% - +5% of nominal voltage. 
On Acti9 offer the min. voltage for test button is given below:

- iID 2P 230V => Min voltage = 175V AC
- iID 4P 400V => Min voltage = 240V AC
- Vigi iC60 230/400V => Min voltage = 205V AC
- Vigi iC60 130V => Min voltage = 110V AC
Was this helpful?
What can we do to improve the information ?