Technical FAQs

Ask a Question

What are the standard openings available for mounting the PK Pratika sockets in Kaedra range of enclosures.

The standard openings which are available for mounting the PK Pratika sockets in Kaedra range of enclosures is given below

-> Mini enclosures for PK sockets >> 65 x 85 mm
 
-> Enclosures for PK sockets >> 90 x 100 mm
 
-> Enclosures for modular devices with interface >> 90 x 100 mm
 
-> Enclosures for interface >> 90 x 100 mm
 
-> Enclosures for PK Unika sockets >> 103 x 225 mm
 
Was this helpful?
What can we do to improve the information ?