Technical FAQs

Ask a Question

Are PK range of Plug and Sockets resistant to fire and abnormal heat according to IEC 60695-2-11 standard.

The PK range of Plug and Sockets are resistant to fire and abnormal heat according to IEC 60695-2-11 standard.

These have been tested for 850ºC as per the glow wire test.
Was this helpful?
What can we do to improve the information ?