Technical FAQs

Ask a Question

What is the electrical endurance class of the Earthing switch used in PIX range of switchboard.

The electrical endurance class of the Earthing switch is class E2 as per IEC62271.
Was this helpful?
What can we do to improve the information ?