Technical FAQs

Ask a Question

Is there any way to order the bushing as spare part for RM6 unit.

RM6 unit has a chamber filled SF6 and sealed for life, so the bushing cannot be replaced because it's assembled before sealing. So there is no way to ordering the RM6 bushing as spare part.
In any case, it is not possible to remove the bushings and if the insert part of the bushing is definitively damaged, the total unit must be replaced.
 
Was this helpful?
What can we do to improve the information ?