Technical FAQs

Ask a Question

Are the 2 ports available on ACE850 module having the same IP address.

Yes, ACE850 has only one IP address used by both P1 and P2 port.

It is possible to use one port or two port depending on the network topology.

Was this helpful?
What can we do to improve the information ?