Technical FAQs

Ask a Question

What are the International standards to which PK Pratika range comply.

The PK Pratika range are in conformity with the international IEC60309-1 and IEC60309-2 standards.
Was this helpful?
What can we do to improve the information ?