Technical FAQs

Ask a Question

What is the default IP address for the M340 MB+ proxy TCSEGDB23F24FA

 The default IP address can be found by converting the last 2 numbers of the MAC address from Hex to Dec and preceding them with 85.16

MAC address 00.80.F4.06.4C.38
4C Hex converts to 76 Dec
38 Hex converts to 56 Dec

Default IP address is
Was this helpful?
What can we do to improve the information ?