Technical FAQs

Ask a Question

How do you memory protect the M340 CPU

The M340 can be placed into memory protect by designating a discrete input in the M340 configuration. The input that you designate must exist and must be hardwired
to allow a toggle between 0>1 or 1>0 for memory protect to be turned off and on. Use only topological references for the memory protect input. It prohibits the transfer of a project into the PLC and modifications in online mode, regardless of the communication channel. The Run and Stop commands are authorized.

Was this helpful?
What can we do to improve the information ?