Technical FAQs

Ask a Question

How to remove or disable the M340 CPU SD memory card

To disable or remove M340 cpu SD card follow the below procedure :-

1. Connect to M340 and make sure the Unity project is Equal, Run and Built.
2. Stop the PLC.
3. Open SD card door.
4. Open the Animation Table Window.
5. Add system bit %S65.
6. Turn on the Modification button.
7. Enter value 1 for %S65. (LED above the SD card will go OUT.
8. Remove the SD card.
Was this helpful?
What can we do to improve the information ?