Technical FAQs

Ask a Question

Do we have substitution kit to fit the Altivar 71 to the old dimension of the Altivar 58 drive.

Refer to attached file for the substitution kit for Altivar 58 .This substitution kit is used to install an Altivar 71 drive in the place of an Altivar 58 drive using the same fixing holes.
Was this helpful?
What can we do to improve the information ?