Technical FAQs

Ask a Question

Which port can be used in Momentum PLC to upgrade its firmware

The Momentum Processor can be upgraded using any of the following 3 options. 

                1. The embedded Ethernet Port

                2. An optional Modbus RS232 serial port (172JNN21032)

                3. An optional Modbus Plus port (172PNN21022 or 172PNN26022)

The firmware is loaded by using the Exec. Loader Utility program.  It is a simple step by step program that allows easy upgrade of the Momentum firmware. 
This program is located in the Concept programming software folder.

Was this helpful?
What can we do to improve the information ?