Technical FAQs

Ask a Question

Can i use PL7 Pro programming software on Windows 7 platform

It is only possible to use PL7 V4.5 SP5 with Windows 7 when used in XP mode. For more info on XP mode refer to below link :-
Was this helpful?
What can we do to improve the information ?