Technical FAQs

Ask a Question

Is it possible to install SoMachine V3.1 and SoMachine V4.1 on same computer system

Yes, Installation of SoMachine v4.1 allows parallel installation of it with SoMachine v3.1 User can install SoMachine V4.1 on same system without un-installing SoMachine V3.1
Was this helpful?
What can we do to improve the information ?