Technical FAQs

Ask a Question

What is the maximum memory size of SD card that M221 controller supports

M221 controller supports SD card up to 32 GB (Maximum) of type SD (Standard capacity) or SDHC (High capacity)
Was this helpful?
What can we do to improve the information ?