Technical FAQs

Ask a Question

What should be the maximum distance between TM3XTRA1 – TM3 bus extension transmitter module and TM3XREC1 - TM3 bus extension receiver modules

Maximum distance should be up to 5 meter between TM3XTRA1 – TM3 bus extension transmitter module and   TM3XREC1 - TM3 bus extension receiver modules
Was this helpful?
What can we do to improve the information ?