Technical FAQs

Ask a Question

Are TM2 IO modules compatible to use with TM3 bus extension modules: TM3XTRA1 – TM3 bus extension transmitter module and TM3XREC1 - TM3 bus extension receiver modules

TM2 IO modules and TM3 bus extension modules: TM3XTRA1 – TM3 bus extension transmitter module and   TM3XREC1 - TM3 bus extension receiver modules
are not compatible. If TM3 bus extension modules used, it is not possible to use TM2 IO modules and vice-versa
Was this helpful?
What can we do to improve the information ?