Technical FAQs

Ask a Question

What is the importance of the battery saver button in BX600CI-IN?

If the "Battery saver mode" is enabled, then it will increase battery life up to two times.

User can also experience consistent run time over a period.

Note: If the "Battery saver mode" is enabled, the load should be >30 Watts.

Was this helpful?
What can we do to improve the information ?