Technical FAQs

Ask a Question

Does BX600CI-IN model have no load shut down option?

BX600CI-IN supports no load shut down feature only when "Battery Saver Button" option is turned on.

Note: If the "Battery saver mode" is enabled, the load should be >30 Watts.
Was this helpful?
What can we do to improve the information ?