Technical FAQs

Ask a Question

Where Vijeo Citect stores it’s real time data and in which format it stores the data.

Vijeo Citect only stores the trend tag data values in his own proprietary database in *.HST files under data folder . Only by using the trend export tool you can covert these HST files into CSV files for further analyzing the data values. If there is any need to store the real time tag values then you have the option to declare that tag as trend tag so that it`s value will be stored in his own proprietary database in form of *.HST files 

Was this helpful?
What can we do to improve the information ?