Technical FAQs

Ask a Question

How can I creating an alarm page for selected critical alarms in Vijeo Citect SCADA

To display your crtitical alarms on a separate alarm page you can configure using Alarm Category. For confguring this kindly follow the below steps : 

1. Create a Alarm Category using Citect Project Editor >> Alarms >> Alarm Category . 

2. Configure a new Alarm Category for example "5" 

3. Now in your alarms use this category number "5" 

4. Create a new graphics page using the "Summary" in Tab Style template. 

5. Now use a button with property of input as "PageAlarm(5)" 

When you press this button it will opens a summary page with Category 5 alarms only which is showing your critical alarms. 

Kindly check the 
attached file for configuration steps.

Was this helpful?
What can we do to improve the information ?