Technical FAQs

Ask a Question

While saving graphics page it take long time and sometimes page goes to not responding condition , how can I resolve this error in Vijeo Citect SCADA

The main reason for this error is that in Vijeo Citect SCADA, is due to the reason that every graphics object that gets added to a graphics page, gets added to the Pgdynobj.DBF database when the page is saved. However when you remove the object, the line of entry for that particular object in Pgdynobj.DBF sometimes do not get removed. Over time you may get a built up of the Pgdynobj.DBF to a very large size. 

In order to reduce the size you can copy the pgtouch.dbf file from your C:\CitectSCADA\User\System or C:\Documents and Settings\All Users\Application Data\Citect\CitectSCADA\User folder over the top of your offending pgtouch.dbf file to zero out the file. 

In Graphics Builder, perform a update pages and in Project Editor, perform a full compile.This should rebuild the information in your pgtouch.dbf file. Using this way we can resolve this error.
Was this helpful?
What can we do to improve the information ?