Technical FAQs

Ask a Question

What is the maximum allowable distance from ATV71 Drive to braking resistor.

The maximum allowable distance from ATV71 Drive to braking resistor is 50 meter.
Need to take care about the cross section of the cable to have a low resistance value.
Also it is advise to use a shielded cable with 2 wire for assure the rule of EMC.
 
Was this helpful?
What can we do to improve the information ?