Technical FAQs

Ask a Question

What will be the DC bus voltage value for ATV71 drive.

The DC bus voltage will be 1.414 of network voltage.
Example : if the Network voltage is 415 V then the DC bus voltage will be 586.81V (1.414x415).
Was this helpful?
What can we do to improve the information ?