Technical FAQs

Ask a Question

Is there any kit available to fit the Altivar 61 to the old dimension of the Altivar 38 drive.

Refer to attached file for Migration document from ATV38 -> ATV61 .There is a substitution kit. 
This substitution kit is used to install an Altivar 61 drive in the place of an Altivar 38 drive using the same fixing holes.
Was this helpful?
What can we do to improve the information ?