Technical FAQs

Ask a Question

What is the maximum cable length for analogue input (AI) or analogue output (AO) for Altivar 71/61 drive.

The maximum length is 100 meter guaranteed with a twisted shielded pair cable.
But it should be longer if the EMC conditions are good and wire section dimensioned  consequently as for a classical 4-20mA current loop.
 
Was this helpful?
What can we do to improve the information ?