Technical FAQs

Ask a Question

Is there any provision for SoMachine Protocol for HMI communication in M221 or SoMachine Basic software.

SoMachine Basic Protocol is available in M221 that can be used as SoMachine Protocol in HMI. For this feature to work you will have to use Vijeo Designer V6.2 onwards which have driver as SoMachine Combo that support SoMachine protocol as it was available in other SoMachine controller as well as SoMachine Basic protocol.
Please take note that you will have to create variable with the same name as defined in SoMachine Basic configuration, automatic variable update feature is not available in SoMachine Basic.
Was this helpful?
What can we do to improve the information ?