Technical FAQs

Ask a Question

Can we upload application program from Magelis HMI's that is being programmed by Vijeo Designer.

Upload from HMI is only possible if you have selected the Include Editor Project check box and selected the Data file to Secondary Drive (CF Card) or Optional Drive (USB stick) prior to download the application into HMI.

If the above has not been done it will not be possible to upload the application from HMI.

For more information please see the video from below link :

https://schneider-electric.app.box.com/s/0i8ea3p1hfubp74q1p4m
 
Was this helpful?
What can we do to improve the information ?