Technical FAQs

Ask a Question

What are the options to read XML file data in Vijeo Citect

You can read data from XML file into Vijeo Citect scada using the below three options are: 

1. In Cicode, you can open the xml file using the fileopen function and search through the data based on certain syntax. 

2. If the XML file has a consistent format, you may be able to go straight to a specific line to get the data, after opening the file as per point number 1. 

3. Using CitectVBA programming if you have some idea of programming in VBA. 
Was this helpful?
What can we do to improve the information ?