Technical FAQs

Ask a Question

What is the cable resistance of Tesys capacitor duty contactors LC1D*K.

To reduce inrush current the resitive cable with connector is used in Tesys capacitor duty contactors LC1D*K.

The cable resistance is 6.88 Ohms per meter. ( Silicable Alsichrom RVS-PFA )
The cable resistance ( including connection ) is 0.78 Ohms +/- 0.05 for LC1DFK, LC1DGK, LC1DLK and LC1DMK ( length 115mm )
The cable resistance ( including connection ) is 1.60 Ohms +/- 0.05 for LC1DPK, LC1DTK and LC1DWK ( 236mm ).

Please refer the below attached file for more information.
Was this helpful?
What can we do to improve the information ?