Technical FAQs

Ask a Question

How to publish Variable created in SoMachine Logic Builder to Vijeo Designer via SoMachine Protocol in SoMachine V4.1 software.

Earlier version of SoMachine was having a object Symbol Configuration that can be used to select and update variable in Vijeo Designer application using SoMachine Protocol.

In version 4.1 of SoMachine things have changed a bit as Symbol Configuration has been out of phase in this version. The steps for performing the same task is as follows:

1. Create you variable in SoMachine Logic Builder.
2. Go to View, Software Catalog and select Variables.
3. Now you can publish the local variables to Vijeo-Designer by selecting them in the right pane.
4. Don´t forget to build ALL.
5. Go back to SoMachine Central and open Vijeo-Designer.
6. In Vijeo-Designer, Right-click on Variables and Import Variables From SoMachine.

Now you could see the all variable that you have published in SoMachine Logic Builder is available in Vijeo Designer.
Was this helpful?
What can we do to improve the information ?