Technical FAQs

Ask a Question

What is the Thermal current Ith of EasyPact TVS GZ1** Motor protection circuit breakers.

The GZ1** is a motor protection device and not AC1 electrical distribution device.
However the maximum current the GZ1** can sustain is the maximum current setting for the reference.
If this current level is exceed which means to overload the thermal sensor and there will be nuisance tripping.
Was this helpful?
What can we do to improve the information ?