Technical FAQs

Ask a Question

How can we change the default location to open/save the application project in SoMachine V4.1

The location for default directory is set to "My Documents" where all the project is by default getting saved and open the same directory location when we click on open project button.

To change this directory :

1. Open SoMachine Central.
2. Click on the button "Modify the System Options".
3. Under System Option window go to General Option tab.
4. Click on Browse button next to the option Preferred Directory for Open/Saved Projects and select new directory from the popup window.
5. Press OK to change to the new directory.

From now onwards your default location will be changed to the new location for open/save projects.
 
Was this helpful?
What can we do to improve the information ?