Technical FAQs

Ask a Question

What is the significance of terminal block (9 & 10) on IM20-H Insulation Monitoring Device for Hospital applications.

The terminal block (9 & 10) on IM20-H Insulation Monitoring Device is 1 A or 5 A CT input for measuring the secondary current of the insulation transformer.
Was this helpful?
What can we do to improve the information ?