Technical FAQs

Ask a Question

What are reasons for Altivar 71 Braking Resistor getting heated up.

(1) As good installation practice, braking resistor must be mounted where Air inlets and outlets must not be obstructed in any way. 
(2)Further, it is exactly mounted on the top of the drive and because of that natural exhaust air.
(3) Wrong selection of braking resistor.
 
Was this helpful?
What can we do to improve the information ?