Technical FAQs

Ask a Question

Does Line choke and Motor choke for Altivar 71 drive have CE Certification.

The certificate CE of motor choke and Line Choke are included in the CE certificate of ATV71.
 Refer to attached certificate. 
All option referenced with VW3xxxxxx are certified CE with this declaration EC of conformity. 
Was this helpful?
What can we do to improve the information ?