Technical FAQs

Ask a Question

What is the reason for the message "Out of memory" in Vijeo Citect when we try to save any graphics page after modification.

This message occurs due to the reason that column width of some dbf files are wrong(eg. Varibale.dbf,advalm.dbf and so on), which leads to error of "Out Of Memory". This may occurs when engineer has open any of these dbf files by third-party software. Kindlydo not use any third-party software to edit dbf files and use our Citect dbf Add-in in excel instead to modify the dbf files. Kindly contact to Schneider Customer Support if any further help required.
Was this helpful?
What can we do to improve the information ?