Technical FAQs

Ask a Question

Can we use a Full Server license with Vijeo Citect SCADA client system. What are the configuration I need to do for this change.

Yes you can use a Vijeo Citect full server license on a client system also, only you need to select "Full License" in the Computer Setup Wizard on the client system.
Was this helpful?
What can we do to improve the information ?